DUG_SmartDim LED Puck Multiwire_WH-01

Disabling Connected Switches

You can disable the mechanical push-button switches, if it is configured with a moment or with switching/dimming functions.
  1. On the Home screen, tap .
  2. Tap Devices > Micromodule - Dimmer > Configure Connected switches (A).
  3. Select the push button which you want to disable.
    • Push Button 1
    • Push Button 2
  4. Tap Unconfigure (B) from the menu, then tap Yes I’m sure to confirm and disable the push-button switch.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.