DUG_SmartDim LED Puck Multiwire_WH-01

Manual operation

When the Puck is connected to a mechanical push button, the connected lighting devices can be controlled manually.

  • Short press the mechanical push button-1 to turn on/off the light.

  • Press and hold the mechanical push button-1 to adjust the dimming level of the light.

NOTE: Some lamps have a starting point. When you turn on the lamp at a low brightness, it quickly gets very bright and then goes back to the lower brightness automatically. This is the behaviour of the lamp and the dimmer can't change it.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.