DUG_SmartDim LED Puck Multiwire_WH-01

Creating a moment

Moment allows you to group multiple actions that are usually performed together. By using the Wiser Home app, you can create moments based on your needs.
  1. On the Home screen, tap > Moments > .
  2. Enter the name of the moment (A).
    TIP: You can choose the cover image that represents your moment by tapping .
  3. Tap Add actions (B) to select the list of devices.
  4. Select the devices (C) you want to add in the moment and tap Done.
  5. Once all the devices are selected, tap Done.
  6. On the Moment creator page, tap the device to set the condition. For example, select Micromodule dimmer.
    • Tap (D) to turn on.
    • Drag the sliding bar up/down to increase/decrease the brightness (E) and tap Set on the upper right corner.
  7. After setting all conditions, tap Save.
    Once the moment is saved, it will appear on the Moments tab. Tap on the moment to enable it.
    TIP: If you want to see the created moments on the Home screen, go to Home > > Home Screen > Moments and enable the Momentstoggle switch.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?