DUG_ELKO - Wiser 16 A Relay for Temperature Control_WH-00

Setting the device location

Using the Wiser Home app, you can assign the Relay in the room (such as bedroom, living room, dining room etc.).
To assign the Relay location:
  1. On the Home screen, tap .
  2. Tap Devices > Climate > 16A Relay > Location (A) to assign the Relay to the existing room or a new room (B) and tap Submit.
    NOTE: You can configure up to 4 Relays in the same room.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.