DUG_ELKO - Wiser 16 A Relay for Temperature Control_WH-00

Selecting the floor sensor

Using the Wiser Home app, you can select the type of floor sensor that you have installed in case of using electric underfloor heating. The floor sensor measures the floor temperature and displays in the app. This option appears only if you have selected the Relay as Control Type.

DANGER
RISK OF FATAL INJURY FROM ELECTRIC SHOCK
The device is not a Safety Extra Low Voltage (SELV) device. The sensors lines are on mains (230 VAC) line.
  • Only use sensors with the appropriate insulation rating.
Failure to follow these instructions will result in death or serious injury.

To select the floor Sensor:
  1. On the Home screen, tap .
  2. Tap Devices > Climate > 16A Relay > Floor Sensor (A) and select the sensor from the list.
    • NTC 10K

    • NTC 12K

    • NTC 15K

    • NTC 33K

    • NTC 47K

    NOTE: Not fitted is selected by default.
  3. Tap OK.

    Once the floor sensor is selected, new options (B) appear in the app.

    • Floor Temperature - It shows the temperature of the floor measured by the floor sensor.

    • Floor Sensor Offset - Allows you to calibrate the floor sensor to match the actual temperature of the floor.

    • Floor Sensor Upper Limit - The upper limit is set to maintain the floor temperature below the set limit.

    • Floor Sensor Lower Limit - The lower limit is set to maintain the floor temperature above the set limit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?