DUG_ELKO - Wiser 16 A Relay for Temperature Control_WH-00

Renaming the device

You can rename the device using the Wiser Home app.
  1. On the Home screen, tap .
  2. Tap Devices > Climate > 16A Relay > Name (A) to rename the device.
    NOTE: Type and icon (B) are both assigned automatically, based on whether you have radiators or floor heating. You will be able to view this only after the pairing is completed.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.