DUG_ELKO - Wiser 16 A Relay for Temperature Control_WH-00

Removing the device

Using the Wiser home app, you can remove the relay from the Wiser system.
To remove the relay:
  1. On the Home screen, tap .
  2. Tap Devices > 16A Relay > Delete (A).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.