DUG_ELKO - Wiser 16 A Relay for Temperature Control_WH-00

Resetting the device

You can reset the Relay to the factory default. It can be reset manually at any time, e.g., when the Hub is replaced.
To reset the Relay:
  1. Press and hold the Set button for > 20 seconds.
    After 15 seconds, the LED flashes red.
  2. When the LED stops flashing red, release the Set button.
    The LED stops flashing upon successful reset of the Relay.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.