DUG_ELKO - Wiser 16 A Relay for Temperature Control_WH-00

About the device

The Wiser 16 A Relay (hereinafter referred to as Relay) is used to control electrical heaters or electric underfloor heating with On/Off commands or Fil Pilote commands. The fil pilote is a single control wire interface for controlling multiple heaters from a Relay. It can control heaters up to 3000 W.
TIP: Pair with ELKO - Wiser Room Thermostat to control electric heaters or electric underfloor heating.

Features of the Relay:

  • Remotely control electrical heating using the Wiser Home app.

  • Boost the room temperature using the ELKO - Wiser Room Thermostat center button.

Diagram of operating elements

  1. Set button

  2. LED

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.