DUG_ELKO - Wiser 16 A Relay for Temperature Control_WH-00

Installing the device

Refer to the installation instruction supplied with this product.
See installation instructions.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The device is not a Safety Extra Low Voltage (SELV) device. The sensors lines are on mains (230 VAC) line.
  • Only use sensors with double insulated cables.
Failure to follow these instructions will result in death or serious injury.

Choosing Suitable Location to Install:

Device positioning

The Relay has to be installed below or to the side of any heat source. It should not be installed behind or above a wall-mounted heater.

Preparation of the mounting surface

TIP: Breakout tabs can be removed to provide 4x extra mounting holes and 2x larger holes for rear cover cable entry.

Floor sensor installation

It is important that the floor sensor is fitted in the correct location in order to read an accurate floor temperature.

  • Floor sensor must be 1 m from edge of the floor, halfway between pipes.

  • Make sure the sensor is not sitting on top of heating pipes.

  • Assemble sensor cable in a plastic conduit with inside diameter of minimum 16 mm.

  • Fix tape to the end of the conduit, cut a slice in the tape to ensure condensation can come out of the conduit.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.