HRB32898–EN10

Individual harmonic

The smart demand controller gives the power quality measurement parameters. The power quality parameters measured are individual harmonic distortion% for V1 V2 V3 / V12 V23 V31, I1, I2, and I3 waveforms.

Harmonics: Percentage of each harmonic divided by fundamental harmonics

where,

Vh = Harmonic Voltage

V1 = Fundamental Voltage

The device measures harmonic distortion from 2nd to 31st level.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?