HRB32898–EN10

Setting up the smart demand controller

The smart demand controller ships with many default values already set up. To change values, navigate to the appropriate screen and enter new values. Use the instructions in the following sections to change values. New values are automatically saved when you exit the screen and accept the confirmation request.

NOTE: On power up, the meter opens to the same menu page that was last accessed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?