HRB32898–EN10

Setting up the System Configuration

To set up the System Configuration:

  1. Press or to move the cursor to point to the parameter you want to modify.
  2. Press [Edit] to update the selected System Configuration.
  3. Press - or + to scroll through a list of different System Configuration values.

    Parameter

    Values

    Description

    Sys Config

    Star,

    Delta,

    2 Phase,

    1 Phase

    Select the appropriate system configuration value you want the meter to display.

  4. Press [OK] to select the System Configuration.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?