HRB32898–EN10

Configuring the CAL LED for energy pulsing using ION Setup

You can use the ION Setup to configure your meter’s LED for energy pulsing.

  1. Start ION Setup .
  2. Connect to your meter
  3. Navigate to I/O configuration > Energy Pulsing.
  4. Select the LED to configure and click Edit. The setup screen is displayed.
  5. Enter a descriptive name for the LED Label.
  6. Configure the other setup parameters as required.
  7. Click Send to save your changes.

    Energy pulsing LED setup parameters available through ION Setup

    Parameter

    Values

    Description

    Mode

    Off, Energy

    Off disables the LED.

    Energy sets the LED for energy pulsing.

    Pulse Wt. (p/k_h)

    1 to 9999999

    When configured for energy pulsing, this defines how many pulses are sent to the LED for every 1 kWh, 1 kVARh or 1kVAh of accumulated energy.

    Channel

    Active Energy Delivered

    Select which accumulated energy channel to monitor and use for energy pulsing.

    Active Energy Received

    Active Energy Del+Rec

    Reactive Energy Delivered

    Reactive Energy Received

    Reactive Energy Del+Rec

    Apparent Energy Delivered

    Apparent Energy Received

    Apparent Energy Del+Rec

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?