Smart demand controller reset
To begin smart demand controller reset setup:
- Press ► to navigate to [Maint] in the menu list.
- Press [Maint].
- Press [Reset].
- Enter your setup password. The default password is 0000.
-
The resets screen appears.
Meter values can be re-initialized using the reset function. Use the directions in the following sections to set up smart demand controller reset values.
Resets
Resets include smart demand controller re-initialization, as well as resets of all values for the following items:
-
Energy - Clears all values for Energy, Quadrant VARh, and Rate Counters
-
Max Demand - Clears all values for Max Demand and Relay Counters
-
Max Min - Clears all values for Max Min
-
TOU - Clears all values for TOU
-
DM Profile - Clears all values for DM Profile
-
DM Sync - Clears all values for Demand
-