HRB32898–EN10

Smart demand controller Rate

To begin smart demand controller Rate:

  1. Press to navigate to [Maint] in the menu list.
  2. Press [Maint].
  3. Press [Setup].
  4. Enter your setup password.
    NOTE: The default password is 0000. See Smart demand controller password setup for information on changing passwords.
  5. Press [OK].
  6. Press to navigate to [Rate] in the menu list.
  7. Press [Rate]. The Rate Setup screen appears.

Use the directions in the following sections to reset the smart demand controller Rate parameters.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?