HRB32898–EN10

Setting up the Start Current

To set up the Start current:

  1. Press to select Start current (mA), then press [Edit] to modify the parameter.
  2. Press + to increase the active digit through the numerals 0-9.
  3. Press to enter the selected value for the active digit and move to the next digit to the left.

    Parameter

    Values

    Description

    Start current (mA)

    05 to 15

    Enter the Start current, in Milliampere.

  4. Continue until all values are selected, then press [OK] to enter the Start current (mA).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?