Smart demand controller password setup
The password to setup and reset are configurable. Passwords must use four numeric characters. The characters are from the US ASCII character set and are not translated or affected by language selection.
- Press ► to navigate to [Maint] in the menu list.
- Press [Maint].
- Press [Setup].
-
Enter your setup password. Then press [OK].
NOTE: The default password is 0000.
- Press ► to navigate to [Pwd] in the menu list.
- Press [Pwd].
- Press ▼ or ▲ to move the cursor ► to point to the parameter you want to modify, then press [Edit].
- Press + to increase the active digit through the numerals 0-9.
-
Press ◄ to enter the selected
value for the active digit and move to the next digit to the left.
Parameter
Values
Description
Setup
0000 to 9999
Sets the password for accessing the meter setup screens.
Reset
0000 to 9999
Sets the password for resetting the meter’s values.
- Continue until all the values are selected, then press [OK] to set the password.