Main Menu
Presentation
The description and content of the menus depend on the IMU. For more information, refer to the documentation for the device connected to the FDM121 display.
For example, if you have an FDM121 display connected to a ComPacT NSX, refer to the ComPacT NSX – MicroLogic 5/6/7 Electronic Trip Units – User Guide.
The menus available in the are as follows:
|
Menu |
Description |
|---|---|
|
The menu provides quick access to the information essential for operation. For more information, refer section Quick View Menu. |
|
|
The menu displays the data made available by the MicroLogic trip unit:
For more information, refer section Metering Menu. |
|
|
The menu is used to control a circuit breaker equipped with a communicating motor mechanism from the FDM121 display. The proposed commands are:
For more information, refer section Control Menu. |
|
|
The menu is used to display:
For more information, refer section Alarms Menu. |
|
|
The menu contains all the FDM121 display setup functions and the operating assistance information:
For more information, refer section Services Menu. |
Navigation
Navigation within the is as follows:







This map is shared between PSE 890, FDM121 User Guide and PSE 1495 NSXTwin Micrologic 567 User Guide