DOCA0088EN-05

About the Document

Document Scope

The aim of this document is to provide installers and maintenance personnel with the information needed to set up and operate the FDM121 front display module for one circuit breaker.

Validity Note

This document is applicable to FDM121 front display module for one circuit breaker associated with circuit breakers:

  • MasterPacT MTZ circuit breakers with MicroLogic X control unit

  • MasterPacT MTZ circuit breakers with MicroLogic Active control unit

  • MasterPacT NT/NW circuit breakers

  • ComPacT NS 630...1600 A and 1600...3200 A circuit breakers

  • PowerPacT P- and R-frame circuit breakers

  • ComPacT NSX 100...630 A circuit breakers

  • PowerPacT H-, J-, and L-frame circuit breakers

NOTE:
  • The information related to the new generation of ComPacT NS and PowerPacT P- and R-frame circuit breakers in this document applies to the existing range ComPact NS and PowerPact P- and R-frame circuit breakers also. The exceptions are mentioned wherever applicable.

  • The information related to the new generation of ComPacT NSX and PowerPacT H-, J-, and L-Frame circuit breakers in this document applies to the existing range ComPact NSX and PowerPact H-, J-, and L-frame circuit breakers also. The exceptions are mentioned wherever applicable.

  • These new ranges are based on the same technical and dimensional architecture as that of the existing range of circuit breakers.

  • The FDM121 display is compatible with MasterPacT MTZ circuit breakers for firmware version 004.000.009 or later.

Online Information

The technical characteristics of the devices described in this guide also appear online. To access the information online, go to the Schneider Electric country website at www.se.com.

The information contained in this guide is likely to be updated at any time. Schneider Electric strongly recommends that you have the most recent and up-to-date version available on www.se.com/ww/en/download/.

General Cybersecurity Information

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Product Related Cybersecurity Information

WARNING
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
  • Change default passwords at first use to help prevent unauthorized access to device settings, controls, and information.
  • Disable unused ports/services and default accounts to help minimize pathways for malicious attackers.
  • Place networked devices behind multiple layers of cyber defenses (such as firewalls, network segmentation, and network intrusion detection and protection).
  • Use cybersecurity best practices (for example, least privilege, separation of duties) to help prevent unauthorized exposure, loss, modification of data and logs, or interruption of services.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Environmental Data

For product compliance and environmental information, refer to the Schneider Electric Environmental Data Program.

Available Languages of the Document

The document is available in these languages:

Related Documents for IEC Devices

Title of documentation

Reference number

Enerlin'X FDM121 – Front Display Module for One Circuit Breaker – Instruction Sheet

QGH80971

Enerlin'X FDM121 - Front Display Module for One Circuit Breaker - Firmware Release Notes

ComPacT NSXMicroLogic 5/6/7 Electronic Trip Units – User Guide

MasterPacT NT/NWMicroLogic A and E Control Units – User Guide

04443724AA

MasterPacT NT/NWMicroLogic 5.0P to 7.0P Control Units – User Guide

04443726AA

MasterPacT NT/NWMicroLogic 5.0H to 7.0H Control Units – User Guide

04443728AA

MasterPacT, ComPacT, PowerPacT Circuit Breakers - Modbus Communication - User Guide

MasterPacT MTZ - MicroLogic Active Control Unit - User Guide

Breaker Communication and Isolation Module (BCIM) for MicroLogic Active Control Unit - User Guide

MasterPacT MTZ - MicroLogic X Control Unit - User Guide

ULP (Universal Logic Plug) System - User Guide

MasterPacT, ComPacT, PowerPacT - Cybersecurity Guide

Enerlin'X IFE - Ethernet Interface for One Circuit Breaker - User Guide

Enerlin'X IFE - Ethernet Switchboard Server - User Guide

Enerlin'X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide

Enerlin'X IO - Input/Output Application Module for One Circuit Breaker - User Guide

You can download these technical publications and other technical information from our website at www.se.com/ww/en/download/.

Related Documents for UL/ANSI Devices

Title of documentation

Reference number

Enerlin'X FDM121 – Front Display Module for One Circuit Breaker – Instruction Sheet

QGH80971

PowerPacT H-, J-, and L-FrameMicroLogic 5 and 6 Electronic Trip Units – User Guide

48940-312-01 (EN)

MasterPacT NT/NWMicroLogic 2.0A, 3.0A, 5.0A, and 6.0A Trip Units – Instruction Bulletin

48049-136-05

MasterPacT NT/NWMicroLogic 5.0P and 6.0P Trip Units – Instruction Bulletin

48049-137-05

MasterPacT NT/NWMicroLogic 5.0H and 6.0H Trip Units – Instruction Bulletin

48049-330-03

MasterPacT MTZ - MicroLogic X Control Unit - User Guide

ULP (Universal Logic Plug) System - User Guide

Enerlin'X IFE - Ethernet Interface for One Circuit Breaker - User Guide

Enerlin'X IFE - Ethernet Switchboard Server - User Guide

Enerlin'X EIFE - Embedded Ethernet Interface for One MasterPacT MTZ Drawout Circuit Breaker - User Guide

Enerlin'X IO - Input/Output Application Module for One Circuit Breaker - User Guide

You can download these technical publications and other technical information from our website at www.se.com/ww/en/download/.

Information on non-inclusive or insensitive terminology

As a responsible, inclusive company, Schneider Electric is constantly updating its communications and products that contain non-inclusive or insensitive terminology. However, despite these efforts, our content may still contain terms that are deemed inappropriate by some customers.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?