Alarms Menu
Definitions
An event is a digital data changing state or any incident detected by the modules of the IMU. Events are time-stamped and logged in the module event history.
An alarm is a type of event that requires a specific attention.
You can associate an alarm with any measurement or event in the IMU.
Each alarm is given a pre-defined priority level:
-
High priority
-
Medium priority
-
Low priority
-
No priority
You can set the alarm parameters and assign priorities with EcoStruxure Power Commission software.
For more information about alarm setup and priorities, refer to the MicroLogic Trip Units User Guides provided in the section Related Documents.
Presentation
Events and alarms are displayed in the menu of the FDM121 display, where you have the choice between two submenus:
-
displays the 40 last events from the connected devices. The events are recorded by the FDM121 display. The event log file is lost in case of FDM121 power loss.
-
displays the alarms detected by the connected devices. They are not lost in case of FDM121 power loss. The alarms are sorted by types which availability depends on the devices connected to the FDM121 display:
|
Range |
Alarm History Options |
|---|---|
|
MasterPacT MTZ circuit breakers with MicroLogic Active control unit |
|
|
MasterPacT MTZ circuit breakers with MicroLogic X control unit |
|
|
|
|
|
Alarm Real-Time Indication and Acknowledgment
The high-priority and medium-priority alarm are indicated in real time on the FDM121 display on a different way. They must be acknowledged also in a different way.
|
Priority |
Indication in real time |
Clearing of alarms |
|---|---|---|
|
High |
|
|
|
Medium |
|
|
Navigation Through the Screens
The procedure for navigating through the screens is as follows:
Pressing the
key in any screen returns to the screen displayed before the message was appeared.
Navigation Through the Submenu
The procedure for navigating through the screens is as follows:
Event or Alarm Screen
A Event or alarm occurrence date
B Event or alarm occurrence time:
-
In hours and minutes in the general screen
-
In hours, minutes, seconds, and milliseconds in the detailed screen
C Event or alarm name
D Key to return to the event log or alarm history
E Event or alarm type:
F Screen number
G Alarm priority level (indicated in the event log only)
H Event or alarm code