DOCA0088EN-05

Password Management

NOTICE
POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY
Use cybersecurity best practices for password creation and management.
Failure to follow these instructions can result in unintended data loss or loss of application function.

General Description

Four passwords are defined, each one corresponding to a level.

A level is assigned to a role:

  • Levels 1, 2, and 3 are used for general-purpose roles, like an operator role.

  • Level 4 is the administrator level. The administrator level is required to write the settings to the ULP modules using the EcoStruxure Power Commission software.

When an FDM121 command is protected by password, you must enter the password of the right level in a dedicated window.

Initial Passwords

The password values set in factory are:

Password level

User profile

Factory setting

Level 1

Services

‘1111’ = 0x31313131

Level 2

Engineer

‘2222’ = 0x32323232

Level 3

Operator

‘3333’ = 0x33333333

Level 4

Administrator

‘0000’ = 0x30303030

Password Modification

Passwords are modified with the EcoStruxure Power Commission software.

Passwords are composed of exactly four ASCII characters. They are case-sensitive and the allowed characters are:

  • digits from 0 to 9

  • letters from a to z

  • letters from A to Z

Password Reset

If the initial passwords have been changed, three cases require to reset the passwords to their factory settings with the EcoStruxure Power Commission software:

  • A password is forgotten.

  • A new module is added in the IMU: for example, an FDM121 display.

  • An inoperative module is replaced in the IMU.

Resetting passwords with the EcoStruxure Power Commission software is only available with the Schneider Electric service user profile.

Password Screen

The Password screen displays when a password protected command is to be accessed and the default level 3 password is modified in the controlled device.

NOTE: The FDM121 display supports only level 3 password.

Entering a Password

The procedure for entering a password is as follows:

Step

Action

1

Use the and keys to increase or decrease the value of the digit. It automatically rolls over from numeric to alphabetical characters.

2

Use the key to move to the next digit. Pressing this key on the fourth digit loops you back to the first digit.

3

Use the OK key to confirm the password. If the password is correct, the given command is sent. Otherwise an error screen is displayed.

4

Use the key to return to the previous menu without sending any command.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?