DOCA0088EN-05

Quick View Menu

Presentation

This map is shared between PSE 890 FDM121 User Guide and PSE 1495 NSXTwin Micrologic 567 User Guide

The Quick view menu presents information that is essential for operating the device connected to the FDM121 display, divided into a number of screens.

The Quick view menu is displayed by default when the FDM121 display is powered up.

The number of available screens and their content depend on the device connected to the FDM121 display. The behavior is the same for MasterPacT, ComPacT, and PowerPacT circuit breakers.

For example, with ComPacT NSX circuit breakers, they depend on:

  • The type of MicroLogic trip unit (A or E)

  • The number of circuit breaker poles (3-pole or 4-pole)

  • The presence of options (ENVT or ENCT)

The screen number and the number of available screens are indicated in the upper right of the display.

Navigation

Navigation within the Quick view menu is as follows:

  • Use the and keys to go from one screen to another.

  • Use the key to return to Main menu.

  • Use the , , and keys to modify how measurements are displayed.

Example of Screens in the Quick View Menu

The following table displays screens 1 to 8 of the Quick view menu for a ComPacT NSX 4-pole circuit breaker equipped with a MicroLogic E trip unit:

Screen

Description

Screen 1 in the Quick view menu displays the following information:

  • The name of the IMU (Aircon FDR on the screen example).

    The name of the IMU is defined with the EcoStruxure Power Commission software or with the remote controller by using the communication network. It can be up to 45 characters long, but only the first 14 characters are visible on the FDM121 display.

  • The open/closed/trip status of the circuit breaker if the BSCM module is present (Open on the screen example opposite).

  • The status of the LED indicators on the front of the trip unit.

  • The long-time protection Ir pickup setting.

  • The current intensity of the most heavily loaded phase (I3 = 217 A in the screen example opposite).

  • The cradle status of the circuit breaker. When two IO modules are connected to the FDM121 display, the FDM121 display does not display the cradle status in case of configuration discrepancy due to cradle application configured in both the IO modules.

Screen 2 in the Quick view menu displays the current, voltage, active power, and frequency:

  • Phase 1 current I1

  • Phase 1 to phase 2 voltage V12

  • Active power total Ptot

  • Frequency F

Screen 3 in the Quick view menu displays the currents:

  • Phase 1 current I1

  • Phase 2 current I2

  • Phase 3 current I3

  • Neutral current IN

NOTE: IN displays the current for neutral applicable breakers.

Screen 4 in the Quick view menu displays the phase-to-phase voltages:

  • Phase 1 to phase 2 voltage V12

  • Phase 2 to phase 3 voltage V23

  • Phase 3 to phase 1 voltage V31

Screen 5 in the Quick view menu displays the phase-to-neutral voltages:

  • Phase 1 to neutral voltage V1N

  • Phase 2 to neutral voltage V2N

  • Phase 3 to neutral voltage V3N

Screen 6 in the Quick view menu displays the powers:

  • Active power Ptot in kW

  • Reactive power Qtot in kVAr

  • Apparent power Stot in kVA

Screen 7 in the Quick view menu displays the energy meters:

  • Active energy Ep in kWh

  • Reactive energy Eq in kVArh

  • Apparent energy Es in kVAh

Screen 8 in the Quick view menu displays:

  • The frequency F in Hz

  • The power factor PF

  • cos ϕ

Intelligent Modular Unit (IMU) Name

For optimum use of the electrical equipment, use the EcoStruxure Power Commission software or the remote controller by using the communication network to assign a name to the IMU relating to the function with which it is associated.

The procedure for displaying the IMU name is as follows:

Step

Action

Display

1

Select the Quick view menu in the Main menu by using the and keys.

Confirm selection of the Quick view menu by pressing the OK key.

2

Screen 1 in the Quick view menu displays the IMU name: Aircon FDR.

The IMU name defined with EcoStruxure Power Commission software or the remote controller can consist of 45 characters maximum, but only the first 14 characters are visible on the FDM121 display.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?