DOCA0088EN-05

Firmware Update

Description

Use the latest version of EcoStruxure Power Commission software for all firmware updates.

After updating the firmware of one device in the IMU, use the latest version of EcoStruxure Power Commission software to check the firmware compatibility between the IMU devices. The Firmware Update table helps you to diagnose and identify all discrepancy issues between the IMU devices. This table also provides the recommended actions relevant to the detected discrepancies.

For more information on FDM121 display firmware versions, refer to the DOCA0150EN•• Enerlin'X FDM121 - Front Display Module for One Circuit Breaker - Firmware Release Notes.

Checking the Firmware Version

You can find the firmware version of the devices in the IMU by using EcoStruxure Power Commission software.

For more information, refer to the EcoStruxure Power Commission Software Online Help.

Updating the Firmware Using EcoStruxure Power Commission Software

Click here to download the latest version of EcoStruxure Power Commission software.

For more information, refer to the EcoStruxure Power Commission Software Online Help.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?