DOCA0088EN-05

Introduction

Description

The FDM121 display shows the measurements, alarms, and operating assistance data from the intelligent modular unit (IMU). The FDM121 display can control the circuit breaker equipped with a motor mechanism or the pre-defined application performed by the IO module.

The FDM121 display is compatible with MasterPacT MTZ, MasterPacT NT/NW, ComPacT NS, ComPacT NSX, and PowerPacT circuit breakers.

FDM121 Display Features

The main features of the FDM121 display are:

  • Display interface for MasterPacT, ComPacT, and PowerPacT circuit breakers

  • ULP compliant for location of the FDM121 display in switchboard

  • Dual ULP interface for easy daisy chain

  • Monitoring and controlling operation of circuit breakers

  • Alarm LED for medium/high priority events

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?