990-91430E-001

Important Safety Instructions — SAVE THESE INSTRUCTIONS

Read these instructions carefully and look at the equipment to become familiar with it before trying to install, operate, service or maintain it. The following safety messages may appear throughout this manual or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.

The addition of this symbol to a “Danger” or “Warning” safety message indicates that an electrical hazard exists which will result in personal injury if the instructions are not followed.

This is the safety alert symbol. It is used to alert you to potential personal injury hazards. Obey all safety messages with this symbol to avoid possible injury or death.

DANGER
DANGER indicates a hazardous situation which, if not avoided, will result in death or serious injury.
Failure to follow these instructions will result in death or serious injury.
WARNING
WARNING indicates a hazardous situation which, if not avoided, could result in death or serious injury.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
CAUTION
CAUTION indicates a hazardous situation which, if not avoided, could result in minor or moderate injury.
Failure to follow these instructions can result in injury or equipment damage.
NOTICE
NOTICE is used to address practices not related to physical injury. The safety alert symbol shall not be used with this type of safety message.
Failure to follow these instructions can result in equipment damage.

Please Note

Electrical equipment should only be installed, operated, serviced, and maintained by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.

A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.

Per IEC 62040-1: "Uninterruptible power systems (UPS) -- Part 1: Safety Requirements," this equipment, including battery access, must be inspected, installed and maintained by a skilled person.

The skilled person is a person with relevant education and experience to enable him or her to perceive risks and to avoid hazards which the equipment can create (reference IEC 62040-1, section 3.102).

FCC Statement

NOTE: This equipment has been tested and found to comply with the limits for a Class A digital device, pursuant to Part 15 of the FCC Rules. These limits are designed to provide reasonable protection against harmful interference when the equipment is operated in a commercial environment. This equipment generates, uses, and can radiate radio frequency energy and, if not installed and used in accordance with the instruction manual, may cause harmful interference to radio communications. Operation of this equipment in a residential area is likely to cause harmful interference in which case the user will be required to correct the interference at his own expense.

Any changes or modifications not expressly approved by the party responsible for compliance could void the user’s authority to operate the equipment.

Electromagnetic Compatibility

NOTICE
Risk of electromagnetic disturbance
This is a product category C2 UPS product. In a residential environment, this product may cause radio inference, in which case the user may be required to take additional measures.
Failure to follow these instructions can result in equipment damage.

Safety Precautions

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Read all instructions in the installation manual before installing or working on this product.
Failure to follow these instructions will result in death or serious injury.
DANGER
hazard of electric shock, explosion, or arc flash
  • Do not install the product until all construction work has been completed and the installation room has been cleaned.
  • Build a clear, permanent, restricted access area around the system.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The product must be installed according to the specifications and requirements as defined by Schneider Electric. It concerns in particular the external and internal protections (upstream breakers, battery breakers, cabling, etc.) and environmental requirements. No responsibility is assumed by Schneider Electric if these requirements are not respected.
Failure to follow these instructions will result in death or serious injury.
DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
The UPS system must be installed according to local and national regulations. Install the UPS according to:
  • IEC 60364 (including 60364–4–41- protection against electric shock, 60364–4–42 - protection against thermal effect, and 60364–4–43 - protection against overcurrent), or
  • NEC NFPA 70, or
  • Canadian Electrical Code (C22.1, Part 1)
depending on which one of the standards apply in your local area.
Failure to follow these instructions will result in death or serious injury.
DANGER
hazard of electric shock, explosion, or arc flash
  • Install the product in a temperature controlled indoor environment free of conductive contaminants and humidity.
  • Install the product on a non-flammable, level and solid surface (e.g. concrete) that can support the weight of the system.
Failure to follow these instructions will result in death or serious injury.
DANGER
hazard of electric shock, explosion, or arc flash
The product is not designed for and must therefore not be installed in the following unusual operating environments:
  • Damaging fumes
  • Explosive mixtures of dust or gases, corrosive gases, or conductive or radiant heat from other sources
  • Moisture, abrasive dust, steam or in an excessively damp environment
  • Fungus, insects, vermin
  • Salt-laden air or contaminated cooling refrigerant
  • Pollution degree higher than 2 according to IEC 60664-1
  • Exposure to abnormal vibrations, shocks, and tilting
  • Exposure to direct sunlight, heat sources, or strong electromagnetic fields
Failure to follow these instructions will result in death or serious injury.
DANGER
Hazard of electric shock, explosion, or arc flash
Do not drill or cut holes for cables or conduits with the gland plates installed and do not drill or cut holes in close proximity to the product.
Failure to follow these instructions will result in death or serious injury.
WARNING
HAZARD OF ARC FLASH
Do not make mechanical changes to the product (including removal of cabinet parts or drilling/cutting of holes) that are not described in the installation manual.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
Chemical hazard
This product can expose you to chemicals including Tetrabromobisphenol A, which is known to the State of California to cause cancer. For more information, go to www.P65Warnings.ca.gov
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
risk of overheating
Respect the space requirements around the product and do not cover the ventilation openings when the product is in operation.
Failure to follow these instructions can result in equipment damage.

Electrical Safety

DANGER
hazard of electric shock, explosion or arc flash
  • Electrical equipment must be installed, operated, serviced, and maintained only by qualified personnel.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices.
  • Turn off all power supplying the UPS system before working on or inside the equipment.
  • Before working on the UPS system, check for hazardous voltage between all terminals including the protective earth.
  • The battery cabinet contains an internal energy source. Hazardous voltage can be present even when the UPS system is disconnected from the utility/mains supply. Before installing or servicing the UPS system, ensure that the units are OFF and that utility/mains and batteries are disconnected.
  • A disconnection device (e.g. disconnection circuit breaker or switch) must be installed to enable isolation of the system from upstream power sources in accordance with local regulations. This disconnection device must be easily accessible and visible.
  • The battery cabinet must be properly earthed/grounded and due to a high leakage current, the earthing/grounding conductor must be connected first.
Failure to follow these instructions will result in death or serious injury.

Battery Safety

DANGER
hazard of electric shock, explosion, or arc flash
  • Battery circuit breakers must be installed according to the specifications and requirements as defined by Schneider Electric.
  • Servicing of batteries must only be performed or supervised by qualified personnel knowledgeable of batteries and the required precautions. Keep unqualified personnel away from batteries.
  • Disconnect charging source prior to connecting or disconnecting battery terminals.
  • Do not dispose of batteries in a fire as they can explode.
  • Do not open, alter, or mutilate batteries.
Failure to follow these instructions will result in death or serious injury.
DANGER
Hazard of electric shock, explosion, or arc flash
Batteries can present a risk of electric shock and high short-circuit current. The following precautions must be observed when working on batteries
  • Remove watches, rings, or other metal objects.
  • Use tools with insulated handles.
  • Wear protective glasses, gloves and boots.
  • Do not lay tools or metal parts on top of batteries.
  • Disconnect the charging source prior to connecting or disconnecting battery terminals.
  • Determine if the battery is inadvertently grounded. If inadvertently grounded, remove source from ground. Contact with any part of a grounded battery can result in electric shock. The likelihood of such shock can be reduced if such grounds are removed during installation and maintenance (applicable to equipment and remote battery supplies not having a grounded supply circuit).
Failure to follow these instructions will result in death or serious injury.
DANGER
Hazard of electric shock, explosion, or arc flash
When replacing batteries, always replace with the same battery module type.
Failure to follow these instructions will result in death or serious injury.
NOTICE
risk of equipment damage
  • Lithium-ion batteries should not be stored beyond 15 months from the date of production. If they are stored for longer the calendar degradation will cause the batteries to be irreversible degraded beyond what is expected – a reduced runtime will be the consequence. Performance guarantee will be measured from the time of deployment or from production date +15 months, whichever comes first. For storage beyond 15 months, contact Schneider Electric.
  • If the UPS system remains de-energized for a long period, Schneider Electric recommends to shut down the battery cabinet completely.
Failure to follow these instructions can result in equipment damage.
CAUTION
risk of PERSONAL INJURY
This product contains electrolyte and other chemicals. If the product is received with external damage that causes a person to come into contact with the electrolyte, please proceed as follows:
  • EYE AND SKIN CONTACT: Immediately flush with plenty of water and seek medical assistance.
  • RESPIRATORY INHALATION: Immediately move away from vaporized gas, get fresh air and rest, and seek medical assistance if necessary.
Failure to follow these instructions can result in injury or equipment damage.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.