990-91430E-001

Position and Interconnect the Battery Cabinets

NOTE: This procedure describes how to position and interconnect several battery cabinets. If your system only has one battery cabinet, you only need to follow step 2 and step 3.
  1. Remove the side panels that are adjacent to the other battery cabinets.
  2. Push the right-most battery cabinet into position. For seismic anchoring, ensure that the rear seismic bracket connects to the rear anchors.

    Rear View

  3. Lower the levelling feet until they connect with the floor - use a bubble-leveler to ensure that the cabinet is level.
  4. Push the second right-most battery cabinet into position, align with the seismic anchoring (if any), and level the battery cabinet as described in step 2 and step 3.
  5. Install the ten interconnection screws (five in the front and five in the rear) between the two battery cabinets.
    NOTE: To reach the five interconnection screws in the rear of the left-most battery cabinet, the left side panel can be removed. Reinstall the left side panel on the left-most battery cabinet after interconnection.
  6. Push the third battery cabinet into position, align with the seismic anchoring (if any), level the battery cabinet, and interconnect with the other battery cabinets as described in step 2, step 3, and step 5. Continue until all the battery cabinets are in place, levelled, and interconnected.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.