990-91430E-001

Prepare for Installation

  1. Remove the indicated cover.
  2. Remove the two transparent covers.
  3. Remove the plate in front of the battery shelves.
  4. Remove the four boxes with accessory kits from the bottom of the cabinet. Refer to Overview of Accessory Kits for more information on the accessory kits.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.