990-91430E-001

Status LEDs

LED Battery Status Description
Normal

The battery breaker is in the OFF (open) position.

Normal

The battery breaker is in the ON (closed) position.

Normal

The batteries are being discharged.

Normal

The batteries are being recharged.

Major alarm

The battery breaker has tripped and is in the OFF (open) position.

Minor alarm

The battery breaker is in the ON (closed) position.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.