990-91430E-001

Download Data Log from the Data Log Kit (Optional)

  1. Remove the cover plate from the data log kit.
  2. Connect a USB device to the USB port. Push and hold DOWNLOAD button for 50 milliseconds to 3 seconds until LED1 (USB) is turned on. LED1 (USB) is blinking (1 second interval) when data is being downloaded to the USB device.
    NOTE: Recommended capacity of USB device is 32GB or more, and file system supports FAT32 (recommended) or NTFS.
    NOTE: Download time takes up to about 80 minutes (eMMC data capacity 24GB, USB file system based on FAT32).
  3. LED1 (USB) turns off when the download is complete. Reinstall the cover plate back to the data log kit.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.