990-91430E-001

Data Log Kit LEDs

  1. Network

  2. CAN

  3. USB

  4. Firmware

Blinking means 1 second interval. Flashing means 50 milliseconds interval.

LED Status Description

CAN blinking

Firmware blinking

CAN data is incoming.

Firmware is operating.

CAN flashing

Firmware flashing

Data is being reorganized due to setting change. Wait until reorganization is complete.

Network flashing

CAN blinking

Firmware blinking

Network is being used when using Data BMS user interface.

USB blinking

CAN flashing

Firmware blinking

Data is being downloaded to USB device for backup.

Firmware blinking

CAN off

Connection error.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.