990-91430E-001

Overview of EPO Signal Cables

Connect the Class 2/SELV signal cables from the building EPO to the rack BMS. Class 2/SELV circuits must be isolated from the primary circuitry. Do not connect any circuit to the EPO terminal block unless it can be confirmed that the circuit is Class 2/SELV.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.