990-915858A-001

Add a New User or Edit an Existing User

  1. From the home screen on the display select Configuration > Display > Security.
  2. Select Add User to add a new user or select Edit User to edit an existing user of the system.
  3. In the Name field, type in the name of the user. Complete with Enter.
  4. In the Pin field, type in a pin code for the user. Complete with Enter.
  5. In the Confirm Pin field, retype the pin code of the user. Complete with Enter.
  6. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?