Troubleshooting
The following is a list of the most common situations where the equipment does not perform as intended, the most likely cause, and a possible corrective action.
If the suggested corrective action does not return the equipment to normal operation, contact Schneider Electric for assistance.
PDU Troubleshooting
| Situation | Possible cause | Corrective action |
|---|---|---|
| The PDU has no input power. | No input source is available. |
Restore the input source. Check the wiring continuity between the PDU input and the input source. |
| Main input circuit breaker MIB/main input switch MIS is tripped because the manual restart key is in the ON position. | Follow Start Up the PDUto start up the PDU. See Set Manual Restart to ON or OFF for the PDU for details about the manual restart function. | |
| Specific output circuit(s) have no power. | Associated branch circuit breaker(s) is OFF. | Turn the branch circuit breaker(s) ON. |
| The wiring between the branch circuit breaker(s) and the equipment is incorrect. |
Check for wiring continuity and correct phase sequence between the branch circuit breaker(s) and the equipment. |
|
| The equipment associated with the branch circuit breaker is operating above the rated load. |
Schedule a load check of the equipment with Schneider Electric; adjust for load balance if possible. |
|
| The branch circuit breaker is inoperable. | Replace the inoperable branch circuit breaker. | |
| No output from the PDU, but the display is active. | The main input circuit breaker MIB is in the OFF (open) position. |
|
| The main input switch MIS is in the OFF (open) position. |
|
|
| Output from the PDU is on, but the display is not active. | Control power fuse(s) is/are blown. | Replace fuse(s). |
| Overvoltage/undervoltage. | Upstream UPS or power conditioner is inoperable. | Correct problem at the power source. |
| Voltage drop due to distance or excessive load on output. | Reduce the distance or reduce the load. |
Alarm Messages
| Display alarm text | Description | Corrective action |
|---|---|---|
| <LX> Phase Loss Alarm |
Line supply phase L1, L2, or L3 loss is detected. |
Check the input source and the affected phase. Check for blown/inoperable fuses. |
| A Circuit Breaker within the Unit has Tripped |
A circuit breaker within the unit has tripped. |
Check the circuit breaker and identify the cause of the tripping. Clear the tripping event and close the circuit breaker. |
| Branch Breaker <position X> Apparent Power Below Minimum |
Branch circuit breaker in position X apparent power is below the minimum threshold. |
Check the power for the affected branch circuit breaker, evaluate the threshold setting, and adjust as per provided specifications. |
| Branch Breaker <position X> Apparent Power Overload |
Branch circuit breaker in position X, apparent power is above the maximum threshold. |
Check the power for the affected branch circuit breaker, evaluate the threshold setting, and adjust as per provided specifications. |
| Branch Breaker <position X> High Current Alarm at Phase <LX> |
Branch circuit breaker in position X, phase L1, L2, or L3 current is above the high threshold. |
Check the current for the affected branch circuit breaker, evaluate the threshold setting, and adjust as per provided specifications. |
| Branch Breaker <position X> Low Current Alarm at Phase <LX> |
Branch circuit breaker in position X, phase L1, L2, or L3 current is below the low threshold. |
Check the current for the affected branch circuit breaker, evaluate the threshold setting, and adjust as per provided specifications. |
| Branch Breaker <position X> Maximum Current Alarm at Phase <LX> |
Branch circuit breaker in position X, phase L1, L2, or L3 current is above the maximum threshold. |
Check the current for the affected branch circuit breaker, evaluate the threshold setting, and adjust as per provided specifications. |
| Branch Breaker <position X> Minimum Current Alarm at Phase <LX> |
Branch circuit breaker in position X, phase L1, L2, or L3 current is below the minimum threshold. |
Check the current for the affected branch circuit breaker, evaluate the threshold setting, and adjust as per provided specifications. |
| Branch Circuit Breaker <position X> Open | The branch circuit breaker in position X is open. | Check the branch circuit breaker and adjust position or alarm settings as per actual installation sequence on distribution. |
| EPO Activated |
The EPO is activated. |
Reset
the EPO, see Reset EPO Alarm or Buzzer.
Check the remote EPO for the room or the fire control panel. |
| Input Breaker Open |
The main input circuit breaker is open. |
Check the main input circuit breaker and adjust follow the instructions provided in PDU Troubleshooting. |
| Input Current High Alarm at Phase <LX> |
The input phase L1, L2, or L3 current is above the high threshold. |
Check the input current for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Input Current Low Alarm at Phase <LX> |
The input phase L1, L2, or L3 current is below the low threshold. |
Check the input current for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Input Current Maximum Alarm at Phase <LX> |
The input phase L1, L2, or L3 current is above the maximum threshold. |
Check the input current for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Input Current Minimum Alarm at Phase <LX> |
The input phase L1, L2, or L3 current is below the minimum threshold. |
Check the input current for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Input Voltage Maximum Alarm at Phase <LX> |
The input phase L1, L2, or L3 voltage is above the maximum threshold. |
Check the input voltage for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Input Voltage High Alarm at Phase <LX> |
The input phase L1, L2, or L3 voltage is above the high threshold. |
Check the input voltage for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Input Voltage Low Alarm at Phase <LX> |
The input phase L1, L2, or L3 voltage is below the low threshold. |
Check the input voltage for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Input Voltage Minimum Alarm at Phase <LX> |
The input phase L1, L2, or L3 voltage is below the minimum threshold. |
Check the input voltage for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| NMC Communication Lost with <X> Meter |
Lost the local network management interface-to-input meter, output meter, or branch meter communication. |
Check the signal cables. Check that the meter is energized and that it has been configured correctly — use the power meter documentation supplied with the power meter. If the alarm persists, contact Schneider Electric. |
| Output Active Power Phase <LX> Overload |
The output active power for phase L1, L2, or L3 is above the selected high threshold. |
Check the output power for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Apparent Power Phase <LX> Below Normal |
The output apparent power for phase L1, L2, or L3 is below the selected minimum threshold. |
Check the output power for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Apparent Power Phase <LX> Overload |
The output apparent power for phase L1, L2, or L3 is above the selected maximum threshold. |
Check the output power for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Current High Alarm at Phase <LX> |
The output phase L1, L2, or L3 current is above the high threshold. |
Check the output current for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Current Low Alarm at Phase <LX> |
The output phase L1, L2, or L3 current is below the low threshold. |
Check the output current for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Current Maximum Alarm at Phase <LX> |
The output phase L1, L2, or L3 current is above the maximum threshold. |
Check the output current for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Current Minimum Alarm at Phase <LX> |
The output phase L1, L2, or L3 current is below the minimum threshold. |
Check the output current for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Frequency Out of Range |
The output frequency is out of range. |
Check the output frequency, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Power Factor Deviation Alarm at Phase <LX> |
Output power factor deviation for phase L1, L2, or L3 exists. |
Check the output power factor deviation for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Voltage High Alarm at Phase <LX> |
The output phase L1, L2, or L3 voltage is above the high threshold. |
Check the output voltage for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Voltage Low Alarm at Phase <LX> |
The output phase L1, L2, or L3 voltage is below the low threshold. |
Check the output voltage for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Voltage Maximum Alarm at Phase <LX> |
The output phase L1, L2, or L3 voltage is above the maximum threshold. |
Check the output voltage for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Output Voltage Minimum Alarm at Phase <LX> |
The output phase L1, L2, or L3 voltage is below the minimum threshold. |
Check the output voltage for the affected phase, evaluate the threshold setting, and adjust as per provided specifications. |
| Transformer High Temperature Alarm |
Temperature at input transformer is higher than the normal range. |
Check that the ventilation of the PDU is not blocked and review the information available from the PDU display to determine if the PDU is overloaded. |
| Transient Voltage Surge Suppressor Alarm |
Transient voltage surge suppressor system requires service. |
Contact Schneider Electric to schedule a maintenance visit. |