990-915858A-001

Restore Default Configuration

  1. From the home screen on the display select Configuration > Restore Defaults.
  2. Select one of the below options:
    • Restart Network Interface: Select this option to restart network interface.
    • Reset All: Select this option to reset all settings to default. You can select to leave out the TCP/IP settings from the reset procedure.
    • Reset Only: Select this option if you only wish to reset parts of the settings to default values. You can select to reset the following settings: TCP/IP, Event Configuration, and Display Settings.
  3. When you have made your selection, tap OK to reset the selected settings to default.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?