990-915858A-001

View the System Configurations

  1. From the home screen on the display, select Configuration > System.
    1. System Output Voltage: 400 V or 415 V as per your system.
    2. Input Protection: Switch or Breaker as per your system.
    3. Output Protection will show as Not Installed.
    4. Input Meter: None or PM5563 as per your system.
    5. Output Meter: HDPM6000 or PM8000 as per your system.
    NOTE: If there are any differences between the listed system configuration and the actual system, please contact Schneider Electric.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?