990-915858A-001

Configure Modbus

Modbus can be configured for the built-in network management card.

  1. From the home screen on the display, select Configuration > Modbus.
  2. For Serial:
    1. Enable or disable Access.
    2. Set the Address to a number between 1 and 247.
      NOTE: Every device on the bus must have exactly the same settings except the Address, which must be unique for every device. No two devices on the bus can have the same address.
    3. Set the Baud rate to 9600 or 19200.
    4. Set the Mode to:
      8, E, 1, or
      8, O, 1, or
      8, N, 1, or
      8, N, 2.
  3. For TCP:
    1. Enable or disable Access.
    2. Set the Port to 502 or a value between 5000 and 32768.
    3. Set the Timeout for the connection to a number of seconds, if applicable.
    4. Enable or disable Keep-Alive if you want the TCP connection to stay open once it has been established.
  4. Tap OK to confirm your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?