990-915858A-001

Edit or Delete a Branch Circuit Breaker

  1. From the home screen on the display, select Configuration > Branch > Edit Breaker.
  2. Select the Position for the branch circuit breaker and select Modify Breaker to edit the branch circuit breaker parameters or Delete Breaker to delete the branch circuit breaker from the configuration.
    NOTE: If an alarm exists for a given branch circuit breaker, you must reboot the display after deleting a branch circuit breaker to clear the alarm(s).
Once a branch circuit breaker has been added, modified, or deleted, the breaker status will update automatically. If the branch circuit breaker status does not update automatically, go to Configuration > Branch and tap Sync Meter to synchronize the branch circuit breaker with the power meter.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?