990-915858A-001

Configure the Input Parameters

  1. From the home screen on the display, select Configuration > Input.
  2. Enable the Breaker Open Alarm, if needed.
  3. Set the Voltage Thresholds for Maximum, High, Low, and Minimum by tapping Enable and setting the percentage.
  4. Tap the > symbol to go to the next page.
  5. Set the Current Thresholds for Maximum, High, Low, and Minimum by tapping Enable and setting the percentage.
  6. Tap OK to save your settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?