Set Manual Restart to ON or OFF for the PDU
DANGER |
|---|
|
Hazard of electric shock, explosion, or arc flash
Always perform correct Lockout/Tagout before working on
the PDU. The PDU will automatically restart when the mains supply
returns unless manual restart is enabled.
Failure to follow these instructions will result in death or serious injury.
|
- Turn the manual restart key to the OFF position to disable manual restart. When the manual restart key is in the OFF position, the main input device will not trip when the upstream power is disconnected. The PDU will restart automatically when the input power returns.
- Turn the manual restart key to the ON position to enable manual restart. When the manual restart key is in the ON position, the main input device will trip when the upstream power is disconnected. The PDU will not restart automatically when the input power returns. To restart the PDU, set the main input device to the ON (closed) position.
- Store the manual restart key in a safe location when not in use.
DANGER