990-91406E-001

Connect the Power Cables in a 10-40 kVA 3:1 384 VDC UPS

  1. Ensure that all disconnect devices are in the OFF (open) position.
  2. Open the front door of the UPS.
  3. Remove the indicated covers.
  4. Route the power cables through the bottom of the UPS.
  5. Connect the PE cable to the PE busbar.
  6. Connect the input cables (L1, L2, L3), bypass cables (L, N), output cables (L, N), and DC cables (DC+, DC-).
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.