990-91406E-001

Location of Disconnect Devices

Locations of Disconnect Devices on the 3:1 UPSs

10-40 kVA 3:1 220 VDC UPS

50-80 kVA 3:1 220 VDC UPS

100-120 kVA 3:1 220 VDC UPS

10-40 kVA 3:1 384 VDC UPS

60-80 kVA 3:1 384 VDC UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.