990-91406E-001

Remove Jumper Busbars in 100-120 kVA 220 VDC UPSs with External Charger

NOTE: This procedure is only applicable to 100-120 kVA 3:1 220 VDC UPSs with an external charger.
  1. Loosen the screws and open the two doors in the top of the UPS.
  2. Disconnect the signal cable from the control board.
  3. Loosen the two screws and flip down the control board panel.
  4. Remove the indicated jumper busbars and refasten the screws (torque to 5 Nm).
  5. Flip the control board panel back to original position and reconnect the signal cable.
  6. Close the two doors and fasten the screws.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.