990-91406E-001

Connect the Signal Cables

  1. Output dry contacts (230 VAC)

  2. External battery temperature input contact (Non-SELV)

  3. BB trip output contact (SELV)

  4. Input dry contacts (SELV)

  5. USB port (SELV)

  6. RS232 port (SELV)

  7. RS485 ports (SELV)

  8. Parallel ports (SELV)

  9. Intelligent slot for SNMP card (SELV)

  1. Ensure that all disconnect devices are in the OFF (open) position.
  2. Remove the indicated cover.

    10-40 kVA 3:1 220 VDC UPS
    10-80 kVA 3:1 384 VDC UPS

    50-120 kVA 3:1 220 VDC UPS

  3. Route the signal cables through the bottom of the UPS as shown below and fasten the signal cables with cables ties.

    10-40 kVA 3:1 220 VDC UPS

    50-80 kVA 3:1 220 VDC UPS

    100-120 kVA 3:1 220 VDC UPS

    10-40 kVA 3:1 384 VDC UPS

    60-80 kVA 3:1 384 VDC UPS

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.