990-91406E-001

Remove the UPS from the Pallet

  1. Move the UPS to the final installation area using a forklift.
  2. Remove the fasteners.
  3. Remove the packaging.
  4. Remove the kick plates.
    NOTE: Save the kick plates.
  5. Remove the screws connecting the UPS to the pallet.
    NOTE: If the parallel kit has been ordered, the parallel kit will be placed under the UPS on the pallet. Save the parallel kit.
  6. Use a forklift to remove the UPS from the pallet and place it in the final installation location.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.