990-91406E-001

Seal the Cable Openings with Fire-proof Putty for IP31 Compliance

NOTE: After connecting all the cables, it is mandatory to seal all the cable openings with the provided fire-proof putty for IP31 compliance.
  1. Follow the manufacturer’s instructions to soften the provided fire-proof putty. Apply sufficient putty around all the cable openings in the bottom of the UPS.
  2. Make sure that all the gaps around the cables are completely sealed. The finished cable openings should look like this.
  3. Reinstall all the covers.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.