990-91406E-001

Overview of Configurations

UIB Unit input disconnect device
SSIB Static switch input disconnect device
MBB Maintenance bypass disconnect device
BB Battery disconnect device
UOB Unit output disconnect device
NOTE: In Schneider Electric literature, 'disconnect device' is used as a generic term covering circuit breakers or switches as their position may vary depending on configuration. Details about the individual configuration are found in the electrical diagram and/or by reading the symbol on the front of each disconnect device.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.