Connect the Power Cables in a Top Cable Entry System
![]() |
---|
Hazard of electric shock, explosion, or arc flash
Perform a total power off of the UPS system before connecting
the battery cables to the battery breaker.
Failure to follow these instructions will result in death or serious injury.
|
- Lockout/Tagout the breaker in the OFF position.
- Connect the PE cable.
- Connect the DC cables (DC+, DC-) from the UPS.
- Install the protection cover over the terminals on the left side of the battery breaker.
- Install the batteries as described in the installation manual supplied with the empty battery cabinet.
- Connect the battery cables (Batt+, Batt-) from the batteries in the empty battery cabinet 1 to the battery breaker.
- Only for installation with two empty battery cabinets: Connect the ground cable from empty battery cabinet 1 to empty battery cabinet 2.
-
Only for installation with two empty battery cabinets: Connect the battery cables (Batt+, Batt-) from the batteries in
empty battery cabinet 2 to the battery breaker.
NOTE: Leave a wiring diagram with battery information on site.
- Install the protection cover over the terminals on the right side of the battery breaker.