990-91378C-001

Installation Procedure

NOTE: The illustrations in this manuals shows installation in an empty battery cabinet. The battery breaker kit can also be installed in a grounded metal box.

One Empty Battery Cabinet and the UPS

Two Empty Battery Cabinets and the UPS

NOTE: The distance between the battery bank and the UPS must not exceed 200 m. Contact Schneider Electric for installations with a longer distance.
  1. Mount the battery breaker kit. Follow one of the procedures:
  2. Connect the signal cables. Follow one of the procedures:
  3. Connect the power cables. Follow one of the procedures:
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?