990-5912E-001

Mount the Maintenance Bypass Panel to the Wall

CAUTION
Risk of injury or equipment damage
  • Mount the maintenance bypass panel to a wall or a rack that is structurally sound and able to support the weight of the unit.
  • Use appropriate hardware for the wall/rack type.
Failure to follow these instructions can result in injury or equipment damage.
  1. Remove the screws and open the inner door in the maintenance bypass panel.
  2. Measure and mark the four mounting hole locations on the wall.
     

    GVSBPSU10K20H

    GVSBPSU20K60H

    GVSBPSU80K120H

  3. Drill holes in the four marked locations and mount the anchor bolts.
  4. Mount the maintenance bypass panel to the wall.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.